This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: Controlling eCAP APWM Output state on emustop

Part Number: TMS320F28377D


Hi,

For ePWM, I can use trip zone input TZ6 to set the ePWM output to a defined state on an emustop (JTAG pausing the processor). I'd like to do the same for an eCAP APWM output that's running at 50% duty cycle, and make sure the output is low when I pause the processor. Is that possible? Looking through the tech ref manual I didn't see anything. Obviously using an ePWM channel is preferable if I need that functionality, but this is for an existing design. Thanks!