Part Number: LAUNCHXL-F28379D
Hello,
I hope you are doing well. I am using the Launchpad to implement an inverter and get the analogue signals out. I can't use the buffered DAC as they are already being used for another purpose and I only have PWM-DAC1/2/3/4 which are mapped to the Typhoon Device that I am working with. I can't use any other pins for getting these analogue signals out. But the problem is that I can't find any example anywhere which shows how to implement DAC using these pins.
I will appreciate it if you can provide any example code which utilizes these pins as DAC for me to work with. I know that these pins have an built-in RC filter too. If I can get an example code i'll be really grateful.
Thanks
-
Hatif