Part Number: TMS320F28379D
Hello,
Does anybody know of a reliable (and potentially recommended by TI) JTAG opto isolation add on module that is compatible with the XDS200?
I work on power converters and this would be useful to cut down on noise. I have a setup with a fully isolated source for the converter so I can earth ground the controls/F28... common point. Having another layer of isolation to the XDS200 would be useful for noise mitigation.
I did some searching on this forum and did not find anything. I did a general web search and it looks like there is a third party XDS200 knock off with isolation available but I would guess that is not a TI sanctioned part.
Blackhawk had a 20pin JTAG isolation module but it looks like that is discontinued.
If anybody has a known working JTAG isolation module they use for the XDS200 on a recent version of CSS and is available to buy online I would greatly appreciate a link.
Thanks for your time,
Bill