This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28384D: maximum input frequency to the PLL

Part Number: TMS320F28384D

Dear e2e team,

In the Migration Between TMS320F2837x and TMS320F2838x at table 3 page 9 the maximum input frequency to the PLL is 20MHz (instead of 25MHz for the F2838x).

In the datasheet of the device at page. 65 is indicated as maximum frequency (from external oscillator) the value of 25MHz.

Which is the correct value?

Thanks,

Giorgia