This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[Concerto] What's the Frequency?

Question:

I see there are "H", "M" and "E" in the Concerto part numbers that seem to indicate possible operating frequencies.  Can you explain?


Answer:

H:

"H" indicates the high end devices. 

Recall that the 28x can run up to 150 MHz. and the M3 is always limited to 100 MHz and is a divide down from the c28x clock (PLLSYSCLK) (Refer to Concerto College: System).    Therefore these part numbers can run either with a maximum C28x clock or a maximum M3 clock:

C28x  M3
150 MHz  75 MHz
100 MHz 100 MHz

 

M:

M is the mid-range device.   The frequencies are limited to 75 MHz for both the C28x and the M3.

 

E:

At the low-end these devices are limited to 60 MHz for both the C28x and the M3.