Part Number: TMS320F28069F
Other Parts Discussed in Thread: MOTORWARE
TI expert: I'm doing the experiment of motorware lab10, and I have a strange problem that needs help. My control board and the main circuit are powered separately. After the motor operates normally, turn off the DC main circuit power supply, and the motor stops running (because the undervoltage protection is set). When the DC voltage is lower than very low (about 5V), turn on the DC main circuit power supply again (at this time, the control circuit still remains powered). When the motor is started, the motor operates abnormally, the motor is unstable, generates high-frequency noise, and the motor current and voltage oscillate, However, if the DC voltage value is higher than a certain value (about 5V), then turn on the DC main circuit power again, and the motor operates normally. gMotorVars.Flag_ enableOffsetcalc/gMotorVars.Flag_ EnableRsRecalc is true by default. View offset_ I/V does not change after the DC main circuit is closed. I cannot further check the relevant status in the while (gMotorVars. Flag_enableSys) loop, because it involves the est function. Can you give me the reason and how to solve it?
Thanks!
Quan