Hi experts,
My customer has tested the compressor under high speed and heavy load(about 10kW) with universal lib, and they need further increase the output power (about 500W) to meet the spec. They already open the OVM and FWC. Is there anything else can help that? (Increase current amplitude or improve position angle accuracy)
With OVM, can they decrease or clear the minCMPvalue which limits the max duty cycle to output higher voltage?
Thanks and best regards,
Jim