Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Changing the method of phase current measurement

Other Parts Discussed in Thread: CONTROLSUITE

I am trying about to change  from the reference design ( HVMotorCtrl+PFCKit) of low side current measurement employing shunt resistors on inverter phase legs to using an isolated approach( LEM current sensor)  on 2 out of 3 phases of a PMSM.  However the rotor does not move when I drive it using exisitng codes which works well with the low side shunt resistor design.  I did notice the current direction and also modified accordingly on the codes of Clark inputs:-

clarke1.As=_IQ15toIQ((int32)(AdcResult.ADCRESULT1<<3)-_IQ15(0.4978))<<1; // HVPM_Sensored code in Controlsuite
clarke1.Bs=_IQ15toIQ((int32)(AdcResult.ADCRESULT2<<3)-_IQ15(0.5039))<<1; // HVPM_Sensored code in Controlsuite

 clarke1.As= _IQmpy(clarke1.As,_IQ(-1));  // added by me to align the current direction
 clarke1.Bs= _IQmpy(clarke1.Bs,_IQ(-1)); //added by me to align the current direction

.........

The PMSM noised significantly however the rotor does not spin. Do I miss something important else to match this change or I did something wrong on the basis of start?

Thanks in advance!

Harvey