Part Number: TMS320C28346
Other Parts Discussed in Thread: TLK3131
Hello to all.
Currently I am looking for an idea to transfer data from a TMS320C28346 optically.
Transmission speed should be at least 100Mbit.
Ethernet protocol is not necessary because it should be a point-to-point connection.
Best connected to the 16bit bus because all other interfaces are occupied.
I had already looked at the TLK3131. But this is very old, 8bit and I was advised not to use it for new designs.
The only requirement is that it should be connected to the parallel bus and that a SFP fiber optic module should be used
and an internal FIFO
Thanks, a lot.
With kind regards
Marcel