Part Number: TMS320F28069
Other Parts Discussed in Thread: C2000WARE
1. HRCAP Example at location C:\ti\c2000\C2000Ware_4_02_00_00\device_support\f2806x\examples\c28\hrcap_capture_pwm is not running as expected, it is stopping at line 372; ESTOP0.
2. How to get the time in seconds using the HCCAPCLK cycles count (HCCAPCNTRISE0 for Normal mode and PeriodWidthRise0 for High-resolution mode ), is dividing the count with HCCAPCLK frequency the correct way?
3. SYSCLKOUT can be maximum 90MHz, and in High-resolution mode HRCAP_Cal() is needed with a frequency range of 98 to 120 MHz; so we cannot provide SYSCLK in High-resolution mode ?