Part Number: CCSTUDIO3
I get this error when trying to use dis6x. Perhaps it is because we use CCS Version: 11.1.0.00011 or maybe because dis6x is only ccs1040 and is not meant for later versions.
c:\work\tools>dis6x C:\work\flash_kernel_c28x_dual_ex1_c28x1\CPU1_RAM\f2838x_codestartbranch_cpu1.obj Disassembly of C:\work\flash_kernel_c28x_dual_ex1_c28x1\CPU1_RAM\f2838x_codestartbranch_cpu1.obj: INTERNAL ERROR: dis6x experienced a segmentation fault This is caused by a defect in the TI Disassembler. TI Customer Support may be able to suggest a workaround to avoid this. Upgrading to the newest version of the compiler may fix this problem. Contact TI in the E2E support forums at http://e2e.ti.com under "Development Tools", "TI C/C++ Compiler". See the link titled "Submitting an issue". We need to see this ENTIRE error message and a complete, reproducible test case including ALL of the command-line options.
Thanks,
John