Part Number: TMS320F280025C
hi experts
in 28002x TRM, I see two PWM SYNCOUT signal description.
first in figure17-7, 2nd in 17-14. they are different from each other. so which on is correct?
thank you very much~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280025C
hi experts
in 28002x TRM, I see two PWM SYNCOUT signal description.
first in figure17-7, 2nd in 17-14. they are different from each other. so which on is correct?
thank you very much~
Hello Matt,
They're actually the same! One is a zoomed-in version of the other. Here's both images side-by-side, with circles around the same spots in both;


In figure 17-14, everything from the 'OR' and earlier in the logic chain is abstracted into being just from the ePWM, and the one-shot latch set signals are similarly simplified to only TBCTL2[OSHTSYNC]. Finally, figure 17-14 doesn't have the final signal being routed to 'Clear Register'. These changes are because figure 17-14 is supposed to explain in simpler terms that specific aspect of the system, while the earlier image is a larger, more complicated and thorough overview. However, they're both ultimately the same content.
I hope that makes sense,
Jason Osborn