This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I understand that TMU's instructions are extended instruction set of FPU(32).
The F2838x has a built-in FPU64. If so, does the TMU built into the F2838x support FPU64 and support trigonometric math calculation with 64-bits resolution?
If anyone knows, please reply.
Thanks.
The TMU hardware and its associated instruction set are different from the FPU64 hardware and its associated instruction set.
Thanks,
Sira
If so, are there any plans to include TMU64 in the next generation of 28X MCU that will be released in the future?
Thanks,
Sang-il