Part Number: C2000WARE
Hi all
I've download 2 times the linux installer for the C2000Ware Version 4.02.00.00.
Both times I could not run the setup files, although the MD5 checksum is correct.
I tried this in several environment:
- on windows using WSL2
- on a Windows Host with a Ubuntu 22.04 docker image
- within a VM Ware Machine running Mint 20.03:
1. using the downloaded image from windows
2. natively downloaded the image again from within the VM
The checksum always was correct:
mblunschi@Host:/home/jenkins/ticcs$ md5sum C2000Ware_4_02_00_00_setup.run
9a0a10f09b7af5efe67fb92a6d5e0215 C2000Ware_4_02_00_00_setup.run
I always ended up with a similar error message:
mblunschi@Host:/home/jenkins/ticcs$ ./C2000Ware_4_02_00_00_setup.run
-bash: ./C2000Ware_4_02_00_00_setup.run: No such file or directory
mblunschi@Host:/home/jenkins/ticcs$
It stays the same when I run it as 'sudo'.
Of course I checked the access rights, which were set correctly. I even tried to run the file with sudo - no change in the result.
I could not find any installation help or manual on the TI homepages.
What might be the problem here?
Thanks for any help