Other Parts Discussed in Thread: C2000WARE
Hi Teams,
My customer is working on a schematics based on F280013x and want to check if there is anything changed compared to F28002x.
We found that like AIO232 must be configured as analog function, otherwise the analog sampling port will be 0.3V higher than the actual value. In addition, floating the 14 Pin can measure 3.3V high level.
(The other AIO pins also have the same high-level 3.3V phenomenon. If the code is not configured, the sampling will be 0.3v higher)
We can understand that AGPIO needs to be configured through the register GPHAMSEL, but we don't understand why AIO also needs to be configured? The default AIO in F280025 is an analog function, has the AIO port changed in F280013x? The customer needs details, otherwise the chip cannot be mass-produced F2800137. Thanks.


Like AIO232 must be configured as analog function, otherwise the analog sampling port will be 0.3V higher than the actual value. In addition, floating the 14 Pin can measure 3.3V high level. So doubt any change here?


From the picture below, By default, these pins function as analog pins and the GPIOs are in a high-impedance state. So AIO default as analog pins, but actually we must configure the register GPHAMSEL.
Could you please explain this difference in description TRM? Thanks.