Part Number: TMS320F28386S
Is is possible to run code that is in upper flash while lower flash is being updated? For instance, updating Flash 1-4 and run code that is in Flash 5.
Thanks,
John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28386S
Is is possible to run code that is in upper flash while lower flash is being updated? For instance, updating Flash 1-4 and run code that is in Flash 5.
Thanks,
John
Hello John,
It is not possible to read or execute code from a flash bank while the same flash bank is being programmed, even if different sectors are being accessed.
Best regards,
Ibukun