Part Number: TMS320F280039C
Other Parts Discussed in Thread: SYSCONFIG
Hi All,
i am interfacing two TMS320F280039C launchpad boards. one as master & another as slave.
i need master configuration 1 byte receive interrupt . no loopback , 500Kbps.
this is my current configuration generated from sysconfig tool:
void SPIA_MASTER_init()
{
SPI_disableModule(SPIA_MASTER_BASE);
SPI_setConfig(SPIA_MASTER_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA0,
SPI_MODE_MASTER, 500000, 8);
SPI_disableFIFO(SPIA_MASTER_BASE);
SPI_clearInterruptStatus(SPIA_MASTER_BASE, SPI_INT_RX_DATA_TX_EMPTY);
SPI_enableInterrupt(SPIA_MASTER_BASE, SPI_INT_RX_DATA_TX_EMPTY);
SPI_disableLoopback(SPIA_MASTER_BASE);
SPI_setEmulationMode(SPIA_MASTER_BASE, SPI_EMULATION_FREE_RUN);
SPI_enableModule(SPIA_MASTER_BASE);
}