This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800137: C28xx_CPU1: Breakpoint Manager: There are not enough resources available?

Part Number: TMS320F2800137


Hi Teams,

My customer is working on a S/W based on F280013x and want to check if there is anything cause the below question. 

The customer breaks the point for single-step debugging, only sets two breakpoints, and when running to a certain function, the console prompts as follows:

C28xx_CPU1: Breakpoint Manager: There are not enough resources available

What is the cause of this? Please tell me how to remove this prompts in the console. And actually the code can works fine, Not sure if there are other effects. Thanks.