Good morning:
I am using CCS 3.3 with 320F2812PFGA microcontroller.
I was trying to implement CRC32 for the uploaded file. There was a checksum example. I modified it so that it would calculate 32. while i was stepping through the code the CPU locked itself. I cannot unlock it. I thought it was just a glitch. The same thing happen on the second board. All the function was doing is reading memory and calculating the CRC32.
As far as I understood from the posts here the CPUs could not be recovered? The are just garbage and have to replaced. Is this correct?
What should I do to avoid this in the future?
Thanks,
Yvon.