Part Number: TMS320F28379D
Other Parts Discussed in Thread: BOOSTXL-3PHGANINV, SFRA
Hi Team,
Bought the entire Dual Motor Development Kit(including BOOSTXL-3PhGaNInv). Two-motor experiments were performed according to the SPRACO3 manual.
After the experiment, it was found that the actual bandwidth could not reach the expected bandwidth. The bandwidth in the manual is 5kHz, but the actual experimental result is only 1kHz:





--
Thanks & Regards,
Yale Li