Part Number: TMS320F280048-Q1
Hi,
In my board, I connected GPIO24 and GPIO32 to 3.3V with pull-up resistors as you can see below. It represents that device default boot mode is FLASH.


However, these pins are also can be configured as EPWM8A-8B. In my digital power application, I need a new time-base counter that is sync. to ePWM4A.
(I won't provide output waveform at those epwm's. I will just use its time-base to generate SYNCPER signals.)
Can I also use safely these GPIO24 and GPIO32 as EPWM?