Part Number: TMS320F28377S
Can a segment of GSx RAM with a length of 4096 WORD in TMS320F28377S be divided into multiple segments? For example, GS5 is divided into 10 segments. The following definitions are made in the. CMD file. Is this method used in segments correct?
//RAMGS5 : origin = 0x011000, length = 0x001000
RAMP00 : origin = 0x011000, length = 0x000040
RAMP01 : origin = 0x011040, length = 0x000040
RAMP02 : origin = 0x011080, length = 0x000040
RAMP03 : origin = 0x0110C0, length = 0x000040
RAMP04 : origin = 0x011100, length = 0x000040
RAMP05 : origin = 0x011140, length = 0x000040
RAMP06 : origin = 0x011180, length = 0x000040
RAMP07 : origin = 0x0111C0, length = 0x000040
RAMP08 : origin = 0x011200, length = 0x000040
RAM5OT : origin = 0x011240, length = 0x000DC0
For FLOAT32 type data defined in C program, can I write and read UINT32 data at this address in assembler?