Hi experts,
In customer design, they use oscillator temperature compensation to maintain high quality communication (SCI and CAN). However, they don't implement the workaround of errata "ADC: Temperature Sensor Minimum Sample Window Requirement", i.e. the sampling window size is not larger than 550 ns.
They want to check:
1. If not implement the errata's advisory, the oscillator compensation will be not right, how large the impact will be?
2. If not compensate the oscillator temperature deviation, is there any serious risk for the communication interface operation?
Since the communication performance will be more significant for bootloader (or OTA will be failed), and the bootloader can't be updated via OTA, so they want to know the impact, and only if the impact is un-avoidable and proposed to be addressed, they will consider to add the compensation and the workaround.
Thanks,
Will