This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025C: what's the input range of the ADC channels, when VDDA is under 3.3V?

Part Number: TMS320F280025C

hi, experts

     may you have a nice day!

       In internal 1.65V reference, I drawed VDDA and VDDIO to 3.0V, and set the ADC input signal to 3.1V, and the conversion result is still correct.

      although it is good to the system, but I am confued that: why the maximal input signal can be above VDDA ?

      hoping for your reply.