This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

piccolo: trip zone

Hi all,

 

I am having some trouble designing a controller for an inverter using piccolo. As compared to DSP it has only 3 nos Trip zone signal where as in dsp there is 6 trip zone for 6 PWM module seperately and also PDPINT signal. Is there any provision in PICCOLO to make arrangement such that each EPWM module can be protected keeping others alive?

Plz help.

Amit

  • Amit,

    Yes. You can configure any ePWM module to accept any TZ signal -- they are all independent.

    For example, PWM1 can be set to trip PWM1A based on TZ2 and TZ3, while at the same time, PWM4 can be set to trip PWM4A and PWM4B based on TZ1 and TZ2.

    In the other hand, Piccolo indeed has less TZs than previos C28x series, that's because TZ4/5/6 are assigned to fixed fault like emulation fail and clock fail. But, it adds three comparators and these outputs can be fed into PWM as an "analog" trip sources like the previous TZs do.

    Hope it helps.

     

    Best regards,

    Ricky Zhang