This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28069 - Running Program From Flash spra958j

Hi,

The sample projects for F28069 in "Running an Application from Internal Flash Memory on the TMS320F28xxx DSP (Rev. J)" are made for cgtools 6.0.1.

I found only cgtools 6.0.0 beta 1 on http://processors.wiki.ti.com/index.php/Compiler_Releases  today.

When will the release 6.0.1 be uploaded?

Thanks, best regards
Massimo

  • Massimo said:

    Hi,

    The sample projects for F28069 in "Running an Application from Internal Flash Memory on the TMS320F28xxx DSP (Rev. J)" are made for cgtools 6.0.1.

    I found only cgtools 6.0.0 beta 1 on http://processors.wiki.ti.com/index.php/Compiler_Releases  today.

    When will the release 6.0.1 be uploaded?

    Thanks, best regards
    Massimo

    Massimo,

    The full release is available via updates through CCS.   I see that the free tools version is not posted, however.   I will let the appropriate folks know. 

    In the meantime, you should be able to run the examples with 5.2.11.

    Regards,

    Lori