Part Number: TMS320F28034
Environment Setup:
OS:
Linux 5.15.0-60-generic
20.04.1-Ubuntu
Code Composer Studio
Version: 12.1.0.00007
TI RTOS:
https://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/tirtos/index.html -> TI-RTOS 2.00.xx - 2.14.xx Product Releases -> 2.12.01.33 -> Concetro -> Linux
----------------------------------------------------------------------------
Please wait while Setup installs TI-RTOS for C2000 2.12.01.33 on your computer.
Installing
0% ______________ 50% ______________ 100%
#########################################
----------------------------------------------------------------------------
Setup has finished installing TI-RTOS for C2000 2.12.01.33 on your computer.chirag@chirag:~/ti$ ls
ccs1210 CCSExternalReferences CCSTargetConfigurations tirex-localserver-3.7.1
chirag@chirag:~/ti$
chirag@chirag:~/ti$
chirag@chirag:~/ti$
chirag@chirag:~/ti$
chirag@chirag:~/ti$ cd ccs1210/
chirag@chirag:~/ti/ccs1210$ ls
ccs 'Code Composer Studio 12.1.0.desktop' xdctools_3_62_01_16_core
chirag@chirag:~/ti/ccs1210$
chirag@chirag:~/ti/ccs1210$
chirag@chirag:~/ti/ccs1210$
Compiler:
I downloaded below compiler and extracted into Linux but not sure how to install it as I don't see any executable files which can install it into specific directory
Also I dont see any linux installer file inside downloaded files . I read in below document that we need to use xdctools_setuplinux_n_nn.bin for Linux setup
https://software-dl.ti.com/targetcontent/legacy_files/targetcontent/rtsc/xdctools_3_15/xdctools_3_15_00_33/exports/docs/rtscpedia/XDCtools_Installation_Guide/XDCtools_Installation_Guide.html
Version:
3.31.00.24 Core for Linux
http://downloads.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/rtsc/3_31_00_24/index_FDS.html
chirag@chirag:~/Downloads/xdctools_3_31_00_24_core_linux/xdctools_3_31_00_24_core$ ls bin config.jar docs eclipse etc gmake include jre package packages package.xdc tconfini.tcf xdc xdctools_3_31_00_24_manifest.html xdctools_3_31_00_24_release_notes.html xs xs.x86U chirag@chirag:~/Downloads/xdctools_3_31_00_24_core_linux/xdctools_3_31_00_24_core$



MCU:
TMS320F28034
Issue:
I recently started working on TI based MCU. I installed above mentioned CCS, RTOS.
After importing project into CCS I am getting build failure:
CDT Build Console:
Buildfile generation error occurred..
Product com.ti.rtsc.TIRTOSc2000 v2.12.1.33 is not currently installed and no compatible version is available. Please install this product or a compatible version.
Build stopped..
Problem Window Result:
Errors:
Description Type
gmake: *** No rule to make target 'build-948570783', needed by 'configPkg/compiler.opt'. C/C++ Problem
gmake: *** No rule to make target 'build-948570783', needed by 'configPkg/linker.cmd'. C/C++ Problem
gmake: Target 'all' not remade because of errors. c28x_power_block_cooling_controller C/C++ Problem
Product com.ti.rtsc.TIRTOSc2000 v2.12.1.33 is not currently installed and no compatible version is available. Please install this product or a compatible version.
xdc.tools.configuro: Error: Can't find the platform package 'ti.platforms.tms320x28'. TI platforms are no longer shipped as part of XDCtools (/home/chirag/ti/ccs1210/xdctools_3_62_01_16_core). Please ensure you are either using a pre-3.30 version of XDCtools or you have added a product that includes your platform support along the path '/home/chirag/ti/ccs1210/ccs/ccs_base;/home/chirag/ti/ccs1210/xdctools_3_62_01_16_core/packages'. Check that this path names a directory containing the necessary platform support and that the platform name is properly spelled.
Warnings:
Description
This project was created using a version of compiler that is not currently installed - 6.4.12 [C2000]. Another version of the compiler will be used during build - 22.6.0.LTS. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="">software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'.