Part Number: TMS320F28386D
Other Parts Discussed in Thread: SYSCONFIG
Hi team,
Here's an issue from the customer may need your help:


As shown in the figure above, if the Device Support feature is used, the system clock tree is configured through the ClockTree Tool. The default crystal used is 25 MHz and the custom board crystal is 10 MHz. How to modify this file through the sysconfig tool? (The customer knows how to configure the clock, but direct modification of the clocktree.h file is not allowed in CCS projects)
Could you help check this case? Thanks.
Best Regards,
Cherry