This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PWM Synchronization connections

Hi,

I need to program a digital controller for a 3-phase inverter. It needs three different PWM signals which should be synchronized with 3 different external signals. I checked F2812, F28335 and F2808, in all of them the input synchronization just for the first instance (ePWM1) comes from an external pin. Is there any DSP that its ePWMs can receive synchronization input from 3 external pins. I mean three slave ePWMs to three external signals.

Thanks