Other Parts Discussed in Thread: TIDA-010054
I am controlling the dual active bridge converter using f2879d. PId controller is implemented using DCL library. I want to know how to change the phase shift value as i have attached the code showing how to channge duty cycle
/* Example_F28069_PID.c
*
* Copyright (C) 2020 Texas Instruments Incorporated - http://www.ti.com/
* ALL RIGHTS RESERVED
*
*/
// header files
#include "F2806x_Device.h"
#include "F2806x_Examples.h"
#include "F2806x_GlobalPrototypes.h"
#include "DCLF32.h"
// function prototypes
extern interrupt void control_Isr(void);
// global variables
long IdleLoopCount = 0;
long IsrCount = 0;
float rk = 0.25f;
float yk;
float lk;
float uk;
DCL_PID pid1 = PID_DEFAULTS;
float Duty;
float upperlim = 0.95f;
float lowerlim = 0.05f;
unsigned int clampactive;
/* main */
main()
{
/* initialise system */
InitSysCtrl(); // [F2806x_SysCtrl.c]
DINT; // disable interrupts
IER = 0x0000;
IFR = 0x0000;
InitPieCtrl(); // initialise PIE control registers [F2806x_PieCtrl.c]
InitPieVectTable(); // initialise PIE vector table [F2806x_PieVect.c]
EALLOW;
PieVectTable.ADCINT1 = &control_Isr; // [F28069_PID_cisr.c]
EDIS;
/* configure ePWM1 */
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
InitEPwm(); // [F2806x_EPwm.c]
EPwm1Regs.TBCTL.bit.CTRMODE = 3; // freeze TB counter
EPwm1Regs.TBCTL.bit.PRDLD = 1; // immediate load
EPwm1Regs.TBCTL.bit.PHSEN = 0; // disable phase loading
EPwm1Regs.TBCTL.bit.SYNCOSEL = 3; // disable SYNCOUT signal
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; // TBCLK = SYSCLKOUT
EPwm1Regs.TBCTL.bit.CLKDIV = 0; // clock divider = /1
EPwm1Regs.TBCTL.bit.FREE_SOFT = 2; // free run on emulation suspend
EPwm1Regs.TBPRD = 0x2328; // set period for ePWM1 (0x2328 = 10kHz)
EPwm1Regs.TBPHS.all = 0; // time-base Phase Register
EPwm1Regs.TBCTR = 0; // time-base Counter Register
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // enable SOC on A group
EPwm1Regs.ETSEL.bit.SOCASEL = 1; // select SOC from zero match
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // generate pulse on 1st event
EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0; // enable shadow mode
EPwm1Regs.CMPCTL.bit.LOADAMODE = 2; // reload on CTR=zero
EPwm1Regs.CMPA.half.CMPA = 0x0080; // set compare A value
EPwm1Regs.AQCTLA.bit.CAU = AQ_SET; // HIGH on CMPA up match
EPwm1Regs.AQCTLA.bit.ZRO = AQ_CLEAR; // LOW on zero match
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
/* configure ADC */
InitAdc(); // [F2806x_Adc.c]
EALLOW;
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 0; // early interrupt generation
AdcRegs.INTSEL1N2.bit.INT1E = 1; // enabled ADCINT1
AdcRegs.INTSEL1N2.bit.INT1CONT = 0; // disable ADCINT1 continuous mode
AdcRegs.INTSEL1N2.bit.INT1SEL = 1; // setup EOC1 to trigger ADCINT1
AdcRegs.INTSEL1N2.bit.INT2E = 0; // enable ADCINT2
AdcRegs.INTSEL1N2.bit.INT2CONT = 0; // disable ADCINT1 continuous mode
AdcRegs.INTSEL1N2.bit.INT2SEL = 0; // setup EOC1 to trigger ADCINT2
AdcRegs.ADCSOC0CTL.bit.CHSEL = 0; // set SOC0 channel select to ADCINA0
AdcRegs.ADCSOC1CTL.bit.CHSEL = 8; // set SOC1 channel select to ADCINB0
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 5; // set SOC0 start trigger on EPWM1A, due to round-robin SOC0 converts first then SOC1
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 5; // set SOC1 start trigger on EPWM1A, due to round-robin SOC0 converts first then SOC1
AdcRegs.ADCSOC0CTL.bit.ACQPS = 6; // set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
AdcRegs.ADCSOC1CTL.bit.ACQPS = 6; // set SOC1 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
EDIS;
/* configure GPIO */
InitGpio(); // [F2806x_Gpio.c]
EALLOW;
GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0; // GPIO34 = I/O pin
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1; // GPIO34 = output
GpioDataRegs.GPBSET.bit.GPIO34 = 1; // GPIO34 = 1
GpioCtrlRegs.GPBMUX1.bit.GPIO39 = 0; // GPIO39 = I/O pin
GpioCtrlRegs.GPBDIR.bit.GPIO39 = 1; // GPIO39 = output
GpioDataRegs.GPBCLEAR.bit.GPIO39 = 1; // GPIO39 = 0
EDIS;
/* initialise controller variables */
pid1.Kp = 9.0f;
pid1.Ki = 0.015f;
pid1.Kd = 0.35f;
pid1.Kr = 1.0f;
pid1.c1 = 188.0296600613396f;
pid1.c2 = 0.880296600613396f;
pid1.d2 = 0.0f;
pid1.d3 = 0.0f;
pid1.i10 = 0.0f;
pid1.i14 = 1.0f;
pid1.Umax = 1.0f;
pid1.Umin = -1.0f;
rk = 0.25f; // initial value for control reference
lk = 1.0f; // control loop not saturated
/* enable interrupts */
PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // enable PIE INT 1.1 (ADCINT1) - [adcisr]
IER |= M_INT1; // enable core interrupt 1 (ADC) - [control_isr]
SetDBGIER(0x0001); // enable real-time debug interupts
EINT; // enable global interrupt mask
EALLOW;
EPwm1Regs.TBCTL.bit.CTRMODE = 0; // PWM1 timer: count up and start
EDIS;
/* idle loop */
while(1)
{
IdleLoopCount++; // increment loop counter
asm(" NOP");
} // while
} // main
/* control ISR: triggered by ADC EOC */
interrupt void control_Isr(void)
{
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
// read ADC channel
yk = ((float) AdcResult.ADCRESULT0 - 2048.0f) / 2047.0f;
// run PID controller
uk = DCL_runPID_C4(&pid1, rk, yk, lk);
// external clamp for anti-windup reset
clampactive = DCL_runClamp_C1(&uk, upperlim, lowerlim);
lk = (clampactive == 0U) ? 1.0f : 0.0f;
// write u(k) to PWM
Duty = (uk / 2.0f + 0.5f) * (float) EPwm1Regs.TBPRD;
EPwm1Regs.CMPA.half.CMPA = (Uint16) Duty;
IsrCount++;
}
/* end of file */