Part Number: TMS320F28379D
Hi,
I would like to use CLB function of TMS320F28379D IC. Is there any special pin for CLB module ? Can I connect the inputs and outputs randomly ?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28379D
Hi,
I would like to use CLB function of TMS320F28379D IC. Is there any special pin for CLB module ? Can I connect the inputs and outputs randomly ?
Thanks.
Hi Alikaan,
Inputs into the CLB primarily come from other peripherals. If you are wanting to use GPIO inputs into the CLB, you can use a combination of the INPUTXBAR and CLB XBARs to route those signals into the CLB.

Please refer to the CLB module in C2000 Academy as this topic of routing inputs into the CLB is covered very well in that resource: https://dev.ti.com/tirex/global?id=c2000Academy
Regards,
Peter