This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: How to reload/restart CPU2 on a CPU1 reload during Debug

Part Number: TMS320F28379D


I have my project set up so that when I START debug on a CPU1 project, CPU2 automatically loads a project and runs.

If during the debug session, I make a small change to the CPU1 project and rebuild, it prompts me to reload the project after the build.  However, the CPU2 project is not reloaded (or restarted).  

How can I configure the GEL file and/or debug settings so that CPU2 is restarted or reloaded + restarted if CPU1 is rebuilt/reloaded during debug?

Thanks!