This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800137: Problem occurs during debugging & Load program process

Part Number: TMS320F2800137

Tool/software: Code Composer Studio

Dear Ti Forum,

we have a brand-new design with a TMS320F2800137 processor on it. Now we are trying to get it working, but we have troubles to flash the processor with the XDS110DAC2 debugger.

Interesting: Problem occurs during debugging & Load program process. always leads to the same error message: 

C28xx_CPU1: GEL Output:

RAM initialization done

C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: Error executing PLL configuration algorithm. Operation cancelled. (0x0)
C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug.
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File: C:\Users\admin\workspace_v12\tidm_02010_dmpfc_0013x\HVAC_REV3P2_3SC_LIB\tidm_02010_dmpfc_0013x_pmsm.out: Load failed.