Part Number: TMS320F28377S
Hi,
I'm trying to communicate the TMS320F28377xS with the DDS AD9833. The MCU works as a master and the DDS as a slave. I only need to send data, therefore I'm using a 3-wire SPI.
When I look at the Oscilloscope, seems to be fine, I can see the correct data been transfered on the falling edge. (Figure bellow. Data 0x5893 (CH2) being transfered on the falling edge, CH1 = SCLK, CH3 = EN).

However, when I transmit this to the DDS I don't get the expected result. So I tried to analyze the waveforms with the Picoscope. Here is the result:

It seems like I'm always missing the last bit (LSB).
Does anyone have any idea how can I fix this?
Here is my actual code:
/**
* main.c
*/
#include "Peripheral_Setup.h"
#include "math.h"
#include <stdint.h>
Uint32 count = 0;
Uint16 data_vector[] = {0x2100, 0x4010, 0x5893, 0xC000, 0x2000}; //Sine - I need 5 writes to get the sine on DDS output
Uint16 rdata;
Uint16* ptr = data_vector;
Uint16 flag = 0;
void spi_xmit(Uint16 a);
void spi_fifo_init(void);
void spi_init(void);
int main(void)
{
//Initializations
InitSysCtrl(); // Initialize System Control:
InitGpio();
//InitSpiaGpio();
EALLOW;
CpuSysRegs.PCLKCR0.bit.CPUTIMER0 = 1;
EDIS;
DINT; // Disable CPU interrupts
InitPieCtrl(); // Initialize the PIE control registers to their default state
IER = 0x0000; // Disable CPU interrupts
IFR = 0x0000; // Clear all CPU interrupt flags:
InitPieVectTable(); // Initialize the PIE vector table
//Functions
Setup_GPIO();
Setup_ePWM();
Setup_ADC();
spi_init(); //Initialize the SPI
spi_fifo_init(); //Initialize the SPI FIFO
EALLOW;
PieVectTable.TIMER0_INT = &isr_cpu_timer0;
//PieVectTable.ADCA1_INT = &isr_adc;
PieCtrlRegs.PIEIER1.bit.INTx7 = 1; //Timer 0
//PieCtrlRegs.PIEIER1.bit.INTx1 = 1; //ADC
EDIS;
IER |= M_INT1;
InitCpuTimers();
ConfigCpuTimer(&CpuTimer0, 200, 0.5); //Not being used
CpuTimer0Regs.TCR.all = 0x4001;
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
//Infinit Loop
while(1){
if(flag !=1){
spi_xmit(ptr[count]);
while(SpiaRegs.SPIFFRX.bit.RXFFST !=1) { }
rdata = SpiaRegs.SPIRXBUF;
count = count+1;
}
if(count>4){count = 0; flag = 1;} //After the 5 writing, no data is transfered anymore
}
return 0;
}
__interrupt void isr_cpu_timer0(void){
//Not being used
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
void spi_xmit(Uint16 a)
{
SpiaRegs.SPITXBUF = a;
}
void spi_fifo_init()
{
SpiaRegs.SPIFFTX.all = 0xE040;
SpiaRegs.SPIFFRX.all = 0x2044;
SpiaRegs.SPIFFCT.all = 0x0;
}
My SPI is configured as follow:
void spi_init(void){
EALLOW;
SpiaRegs.SPICCR.all =0x00DF;
SpiaRegs.SPICTL.all =0x001E;
SpiaRegs.SPIBRR.all =49; //Baud rate = 1MHz
SpiaRegs.SPIPRI.bit.FREE = 1;
EDIS;
}
Thanks in advance!