Problem:
1. I have configured all the channels of ADCC and ADCA, then i have attached a pod to ADCA0/ADCC15 pin of ADC Channel for varying the ADC value and observing the value through debugger.
2. The value of ADCA0/ADCC15 is changing as we are varying the pod from 0 to 4096. while varying the pod, other pins are also changing the values but they are not connected to any external devices.
3. A11/C0 and A12/C1 Registers , which are changing the values.
Questions:
1. May i know why they are effecting while only pin (A0/C15) is connected to pod..? what could be the Reason for it?