Part Number: TMS320F280025C
Other Parts Discussed in Thread: C2000WARE, CCSTUDIO, SYSCONFIG
hi experts,
CCS v12.2, when i import projects with syscfg, The result is as below, what can i do to get syscfg work?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Matt,
Can you please try to import any project from C2000Ware SDK (not Digital Power SDK)?
C:/ti/c2000/C2000Ware_4_03_00_00/driverlib/f28002x/examples/led
I want to check if this example works for you or not.
Regards, Santosh
Matt,
Internet connectivity should not matter.
I tried on MacBook and also on Linux It seems to work on both machine. What is your setup?
Can you open the project setting and check the SysConfig basic options. Does it show anything like this?

OS: WIN10 Pro version 22h2
CCS: v12.2.0.00009
c2000 ware V4.03
here is the SysConfig basic options:

add: I found one important thing:CCS view Resource Explorer offline can not be open, the problem is as same as SysConfig;

OS: WIN10 Pro version 22h2
CCS: v12.2.0.00009
c2000 ware V4.03
here is the SysConfig basic options:

add: I found one important thing:CCS view Resource Explorer offline can not be open, the problem is as same as SysConfig; maybe the problem is in the browser or my computer encrpytion software prohibit one of the browser's application processes.

Matt,
Looks like some dependencies was not installed properly when installing CCS.
Can you please see the below link regarding the MSVC redistributable libraries:
Let me know if it helps.
Regards, Santosh
hi santosh,
Today I reinstalled the computer windows and the CCS, then everything is normal and works well.
Thank you for your attention for so many days to my problems. Maybe you are right so i think this problem solved.
best wishes! may you have a nice day!