This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320LF2403A: input clamp protection

Part Number: TMS320LF2403A

IN the datasheet for the 2403, it says on page 71 that all inputs are protected with a clamp diode to up to 20mA. Does this apply to ALL inputs digital AND analog?

We have a 5k resistor in line with the A/D inputs and a client that wants to put 24 volts in to the board. Our input circuit would limit the current to about 3mA. Is that acceptable even if the input is 24 volts?

Thanks, 

David