Hello, everyone. I have the problem that the target board with 2812 DSC cannot connect the Emulator.
The Emulator is TDS510USB Plus which was produced by Wintech in Beijing, China. And the Emulator
can connect the target board with 28335 DSC which I designed early.
The 3.3V and 1.9V voltage of the 2812 is correct. The XRS signal is High Level after power up. The
JTAG connect is the same as the below, the Vddio is 3.3V voltage.

But the Emulator cannot connect the target board, and the CCS Error information is:

Where is the problem?
Thanks for your attention!