Part Number: TMS320F28052
Hi, I have an issue with my debbuger, an XDS110 debug probe connecting to the F28052 micro-controller.
I am able to connect to the micro and flash the program into it, but whenever I enable the micro to begin running an applicaton (Motor control), I lose connection to the microcontroller.
The following errorr is generated when that happens.
C28xx: Error: (Error -1135 @ 0x3F1438) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.4.0.00129)
C28xx: Unable to determine target status after 20 attempts
C28xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
Please help with what might be the issue.