Part Number: TMS320F28335
Hi There!
I am a TMS320F28335 user. I need more memory.
There is too much '.ebss' data, so RAM block L0 ~ L7 is integrated, but it is still not enough.
Currently, 95% of the RAM area is used, and there are still variables that I have not declared.
In this case, is there an area that I can use instead? help me plz..
ex. SRAM_DATA or ZONE7? (Neither in use)