Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: question on SDFM clock

Part Number: TMS320F280039C

Hi Champs,

F280039C has two SDFM modules, each SDFM module has 4 independent data input (SD-Dx) / clock input pins (SD-Cx).

Due to external signal processing, there will be a delay between the SDFM input and the input signal after the output, and their clocks(CLK_1305 and CLK_back in the picture) are not synchronized, so there will be a feedback clock signal (CLK_back, 20MHz), can the feedback clock CLK_back be used as an input pin of SD-Cx? Customer want to know if it is achievablethat when SDFM sending data, clock uses CLK_1305, and when SDFM receivinging data from AMC1305, clock uses CLK_back? Thanks!

Best Regards,

Julia