Hi,
I am using F2810 and XDS510USB emulator.
I am new to this Code Security function.
Today, I used On-chip Flash Programmer, changed the Key 0 ~ Key 7 to FFF0 and successfully did the "Program Password". Then I flashed the .out file.
However after cycling power, I can not flash the F2812 anymore.
When I clicked "Unlock" with correct password, the On-Chip Flash Programmer window showed me unlocked. But when I click "Execute Operation" to erase the sectors or flash the .out file, the On-Chip Flash Programmer window just went grey. The target board behaved just like been reset and run.
Anyone can help?
Thanks.
Charmaine