Other Parts Discussed in Thread: SYSCONFIG
Hi,
1) I am using an example for F280039C like "adc_ex10_multiple_soc_epwm" and everything is OK
2) Now I want to use the F280037 device (64 pins) instead and do a "SWITCH" in the Sysconfig from F280039C_100PZ to F280037_64PM
3) It seems to give some error but ok, I remove all ADCs and I can recompile.
4) Now, I try to add ADC and enable few SOC and get these error:

Can you help on this please? I need to be able to define the schematics with some other peripheral.
Thanks,
Arnaud