This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386D: cmd grammar

Expert 2480 points

Part Number: TMS320F28386D

When do the memory assignment, shall modify the cmd file as below shows.

Question: Does TI have the related cmd grammar document which can be refer to?

CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start

MEMORY
{
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x000000, length = 0x000002
BOOT_RSVD : origin = 0x000002, length = 0x0001A7 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x0001A9, length = 0x000257
RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RAMD0 : origin = 0x00C000, length = 0x000800
RAMD1 : origin = 0x00C800, length = 0x000800

// CLA data
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800

// CLA ram
RAMLS2_7 : origin = 0x009000, length = 0x003000

/*
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800

RAMLS6 : origin = 0x00B000, length = 0x000800
RAMLS7 : origin = 0x00B800, length = 0x000800
*/
RAMGS0 : origin = 0x00D000, length = 0x001000

RAMGS1_6 : origin = 0x00E000, length = 0x006000
RAMGS7_8 : origin = 0x014000, length = 0x002000
RAMGS9_10 : origin = 0x016000, length = 0x002000

/*