Part Number: TMS320F28075
Hi, I want to use the SQRTF32 TMU intrinsic function in a project, but receive "warning #225-D: function "sqrt" declared implicitly" during compilation. I am following the paradigm of adding two underscores and changing the instruction to lowercase to call it in C like so __sqrtf32(test). I haven't had any issues with the other TMU intrinsic functions in my project (such as __cospuf32, __atan2puf32, etc.). I am using compiler version TI v22.6.0.LTS and Code Composer 12.2.0.9.