Part Number: TMS320F280037C
Other Parts Discussed in Thread: TMS320F2800137
Hi Experts,
We are reviewing the C2000 microcontrollers for potential use in a product.
Parts in this family of microcontrollers seem to have a part number format of TMS320F2800nnn-nn, where the nnn-nn is a combination of numbers and letters. We are wondering if two parts from the TMS320F2800 family are available in the same package, e.g., 48 pin LQFP (PT), does that mean they are a pin-to-pin compatible? As an example, if the TMS320F2800137 in the 48 pin LQFP (PT) package is initially designed into a product, is the TMS320F280037C-Q1 in the 48 pin LQFP (PT) a pin-to-pin compatible part?
In this example, the TMS320F2800137 is a non-automotive / non-safety rated component. Should the need arise for an automotive grade / safety rated microcontroller, it would be good to know if a pin-to-pin compatible device in the same product family is available. There are other examples of this, too. For example, some of the parts in the TMS320F2800nnn-nn are available in the 64 pin LQFP (PM) package.
Are other TMS320F2800nnn-nn parts in the 64 pin LQFP (PM) package considered pin-to-pin compatible?
We are aware with the comparison tables and pinouts packages, but we would like to confirm it from an experts especially those options with "Configurable logic block" feature.
Thank you for your guidance.
Regards,
Archie A.