Hi all,
I was able to flash my 320F28335 when it was set to "Jump to Flash" option.
I am trying SCI bootloader option ( by changing GPIO to SCI-A boot option). After this change my processor does not boot up.
I downloaded my code using JTAG interface and it only works well until it has power. As soon as it restarts, it is unresponsive. ( Whereas it was was working well when I had "Jump to Flash" option. )
So far as i understand, SCI bootlaoder is built in to the processor and if dosen't get any serial data (0x08AA) it will jump to "FLASH_ENTRY_POINT" where it calls my Watchdog disable routine and runs the code.
I also tried loading my code with bootlader which successfully erases Flash and programs it but after power cycle same response, no any activity.
Can someone please help me with this.
Regards