This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: C2000 Hex Utility, how to use "--fill" and "--image"

Part Number: TMS320F28035

**** Build of configuration Debug for project OBC_F28032 ****

"D:\\ti\\ccs1220\\ccs\\utils\\bin\\gmake" -k -j 16 all -O

Building file: "../SOURCE/KADD008U1_SciBoot.c"
Invoking: C2000 Compiler
"D:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="E:/0.MCU_Code/00.CCS12/OBC_F28032/OBC_F28032" --include_path="D:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --include_path="E:/0.MCU_Code/00.CCS12/OBC_F28032/OBC_F28032/INCLUDE" --advice:performance=all -g --diag_warning=225 --diag_wrap=off --display_error_number --abi=coffabi --preproc_with_compile --preproc_dependency="SOURCE/KADD008U1_SciBoot.d_raw" --obj_directory="SOURCE" "../SOURCE/KADD008U1_SciBoot.c"
Finished building: "../SOURCE/KADD008U1_SciBoot.c"

Building target: "OBC_F28032.out"
Invoking: C2000 Linker
"D:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --advice:performance=all -g --diag_warning=225 --diag_wrap=off --display_error_number --abi=coffabi -z -m"OBC_F28032.map" --stack_size=0x200 --warn_sections -i"D:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/lib" -i"D:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" -i"E:/0.MCU_Code/00.CCS12/OBC_F28032/OBC_F28032" --reread_libs --diag_wrap=off --display_error_number --xml_link_info="OBC_F28032_linkInfo.xml" --entry_point=_B1_Rst_Entry --rom_model -o "OBC_F28032.out" "./INCLUDE/KADD008U1_IsrVariableDefs.obj" "./SOURCE/DSP2803x_Comp.obj" "./SOURCE/DSP280x_Adc.obj" "./SOURCE/DSP280x_CSMPasswords.obj" "./SOURCE/DSP280x_CodeStartBranch.obj" "./SOURCE/DSP280x_CpuTimers.obj" "./SOURCE/DSP280x_DBGIER.obj" "./SOURCE/DSP280x_DefaultIsr.obj" "./SOURCE/DSP280x_DisInt.obj" "./SOURCE/DSP280x_ECan.obj" "./SOURCE/DSP280x_EPwm.obj" "./SOURCE/DSP280x_GlobalVariableDefs.obj" "./SOURCE/DSP280x_Gpio.obj" "./SOURCE/DSP280x_I2C.obj" "./SOURCE/DSP280x_InitPeripherals.obj" "./SOURCE/DSP280x_MemCopy.obj" "./SOURCE/DSP280x_PieCtrl.obj" "./SOURCE/DSP280x_PieVect.obj" "./SOURCE/DSP280x_Sci.obj" "./SOURCE/DSP280x_SysCtrl.obj" "./SOURCE/DSP280x_usDelay.obj" "./SOURCE/GBB_EntryVect.obj" "./SOURCE/GBB_epromdata.obj" "./SOURCE/GBB_main.obj" "./SOURCE/KADD008U1_Isr.obj" "./SOURCE/KADD008U1_SciApp.obj" "./SOURCE/KADD008U1_SciBoot.obj" "./SOURCE/KADD008U1_cal.obj" "./SOURCE/KADD008U1_initial.obj" "./SOURCE/KADD008U1_start.obj" "./SOURCE/KADD008U1_vAdcTreatment.obj" "./SOURCE/KADD008U1_warnctrl.obj" "../2803x_FlashAPI_BootROMSymbols.lib" "../DSP2803x_Headers_nonBIOS.cmd" "../F28032.cmd" "../IQmath.lib" "../SFO_TI_Build_V6.lib" -llibc.a -l"E:/0.MCU_Code/00.CCS12/OBC_F28032/OBC_F28032/IQmath.lib" -l"E:/0.MCU_Code/00.CCS12/OBC_F28032/OBC_F28032/2803x_FlashAPI_BootROMSymbols.lib"
<Linking>
"../F28032.cmd", line 157: warning #10068-D: no matching section
"../F28032.cmd", line 161: warning #10068-D: no matching section
warning #10063-D: entry-point symbol other than "_c_int00" specified: "_B1_Rst_Entry"
Finished building target: "OBC_F28032.out"

Building secondary target: "OBC_F28032.hex"
Invoking: C2000 Hex Utility
"D:/ti/ccs1220/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/hex2000" --fill=0xFFFF --image --memwidth=16 --romwidth=16 --diag_wrap=off --intel -o "OBC_F28032.hex" "OBC_F28032.out"
makefile:189: recipe for target 'OBC_F28032.hex' failed
error: -image requires ROMS directive
gmake[1]: *** [OBC_F28032.hex] Error 1
gmake[1]: Target 'secondary-outputs' not remade because of errors.
makefile:178: recipe for target 'all' failed
gmake: *** [all] Error 2

**** Build Finished ****