Part Number: TMS320F28069
I am using HRCAP Type 0 for 2803x and 2806x.
When I give input to the HRCAP Pin externally through the function generator then it detects the signal correctly
If I give a signal through the ePWM block and then connect the pin from ePWM externally to the HRCAP pin, Calibration never happens (status =0 always ) unless I do TBCLKSYNC=1 before calling the HRCAP calibration function.
I can observe the same in example_2806xHRCAP_HRPWM if I manually set PCLKCR0 to 0x5719 ( TBCLKSYNC=0) after line 262 (HRPWM_Config() which makes TBCLKSYNC=1 ), then calibration doesn't happen with status as 0 always.
so my doubt is, is it necessary to make TBCLKSYNC=1 before doing HRCAP_Cal(), if we are using ePWM to generate the waveform?