This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386D: Debug error

Expert 2420 points

Part Number: TMS320F28386D

When do the debug, CCS often give the below error remind, and the debug failed.

We use the XSD110 which bought from TI.

What is the problem it maybe?

C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.6.0.00172)
C28xx_CPU1: Trouble Halting Target CPU: (Error -1135 @ 0x8739) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.6.0.00172)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging

  • Hi W Z,

    The expert is currently out of office, please expect a response back by tomorrow.

  • Hi,

    Could you please use the 'Test Connection' button in your Target Configuration (.ccxml) file? Please post the output log here. Could you also try putting the device in 'wait boot' mode then see if you are able to connect? The below table from the datasheet describes how to do this. 

    Best Regards,

    Ben Collier

  • CS_DAP_0: Error: (Error -242 @ 0x0) A router subpath could not be accessed. The board configuration file is probably incorrect. (Emulation package 9.6.0.00172)
    C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.6.0.00172)
    C28xx_CPU1: Trouble Halting Target CPU: (Error -1135 @ 0x19411) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.6.0.00172)
    C28xx_CPU1: Unable to determine target status after 20 attempts
    C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
    C28xx_CPU2: Can't Run Target CPU
    C28xx_CPU2: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.6.0.00172)
    C28xx_CPU2: Error: (Error -1135 @ 0xFC5C) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.6.0.00172)
    C28xx_CPU2: Unable to determine target status after 20 attempts
    C28xx_CPU2: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
    Cortex_M4_0: JTAG Communication Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.6.0.00172)

  • Hi,

    Could you please post a screenshot of your target configuration file like shown below? Your target configuration file should look like below, but with XDS110 and F28386D selected. 

    Best Regards,

    Ben Collier  

  • My DSP is TMS320F28386D

  • Hi,

    Are you able to see your debugger in your computer's device manager? Do you have access to any other C2000 boards? Are you able to connect to other C2000 devices with your XDS110 debug probe? If not, could you please try following the steps from this webpage to update your XDS110's firmware? https://software-dl.ti.com/ccs/esd/documents/xdsdebugprobes/emu_xds110.html

    Best Regards,

    Ben Collier